A vision of mobility is emerging in which vehicles not only deliver clean transportation, but also store excess energy from renewable sources. New drive systems, battery, billing, and smart grid technologies are setting the stage for tomorrow's energy and transportation ecosystem..
Font Size


Imagine millions of electric vehicles in parking lots and garages, each drawing power from the grid. Now take the thought one step further and imagine each vehicle returning some of its stored energy to the grid during periods of peak power demand. That's the vision that is set to transform the automotive industry over the next few years. It's a vision that is not possible with the internal combustion engine. However, it can be achieved with a bidirectional battery that can be charged up or used as an energy source.
This vision of electric mobility has come about as the result of the convergence of a number of factors. An increasing number of people want to be mobile, while energy consumption is rising dramatically, especially in emerging markets such as India and China. In the past, these demands were met mainly by using fossil fuels. And indeed, for over 100 years cars have been powered by combustion engines while electrical power has essentially been produced by burning coal or natural gas.
Time is running out, however, because fossil resources are being depleted, and the CO2 emissions they produce are accelerating climate change. More and more energy suppliers are therefore utilizing renewable and CO2-free energy sources, such as wind and solar power. The problem here, however, is that their yield depends on the weather. As the share of electricity from such sources increases, so too does the need to develop interim storage facilities whose energy can be tapped at a moment's notice. One idea is to use batteries in electric cars, which, depending on demand for electricity and price, can either be recharged from any power outlet or return electricity to the grid. If, for example, a surplus of electricity is available, as is often the case at night or during periods of windy weather, prices could be lowered, making it attractive to "fill up" at such times. Conversely, if winds were calm, or a lot of electricity was being used during the day, the price might rise accordingly, which would lead many vehicle owners to sell their electricity back to the grid at a profit.
In fact, an intelligent management system installed in each car could even make the decision itself, provided it knew how far its driver planned to travel that day, and how much electricity the battery would require for that distance. In any case, most cars sit idly for most of the day, which means they could be continually connected to the grid from their office parking spaces, parking lots or home garages. Flexibly determining electricity prices in accordance with supply and demand would also eliminate any problem associated with many vehicles trying to recharge at once, which of course would cause prices to skyrocket.
The rule of thumb is that there should be some 300 electric vehicles as potential energy storage units for every wind turbine with a peak output of three megawatts. The existence of cars as mobile storage units would kill two birds with one stone. Assuming vehicle batteries could handle numerous charging and discharging cycles, energy supply companies would be provided with a buffer against surplus energy from renewable sources, while vehicle owners would have a source of income to help them finance their relatively expensive batteries.
In the foreseeable future, batteries will remain one of the most expensive components in electric cars. Achieving a range of 100 km for a mid-sized vehicle today requires a battery with approximately 15 kWh of energy content. Such a battery currently costs more than €10,000. However, there are other options for such mobile power plants besides having them financed through income from electricity. For one thing, vehicle owners wouldn't necessarily have to buy the battery. Instead, it could be leased from an energy supplier. In other words, an energy company would decentralize its energy storage capacity and finance the battery through the latter's "secondary use."
Regardless of what form electric cars may take, and what role they will play in the electricity mix, any future concept will need to incorporate the most important stakeholders: electricity producers, automakers, suppliers, and governments, whose policies should pave the way for the necessary paradigm change.
In Germany, a first step was taken in November 2008, when the Ministry of Economics and Technology (BMWi); the Ministry of Transport, Building, and Urban Affairs (BMVBS); the Ministry for the Environment, Nature Conservation, and Nuclear Safety (BMU); and the Ministry of Education and Research (BMBF) held a National Strategy Conference on Electric Mobility. The conference brought together energy suppliers such as E.ON, RWE, and Evonik; automakers and suppliers such as Volkswagen, Daimler, Continental, and Bosch; electrical and electronics companies such as Siemens; and various research institutes. "My goal is to utilize electric mobility to help achieve a breakthrough for a new culture of mobility and a new system of urban planning," said German Transport Minister Wolfgang Tiefensee at the conference. Environmental Minister Sigmar Gabriel added that electric cars acting as buffer storage units would establish an important link to renewable energy sources.
Such a development will become important in Germany, Gabriel said, because the country plans to increase the share of renewable energy sources in its electricity mix from around 15 % today to as much as 40 % by 2020. Secretary for Economics and Technology Dagmar Wöhrl added that it is essential for utilities to work closely with automakers, as extensive R&D investment will be required—particularly in the fields of energy storage, vehicle engineering, and power-grid integration.
In fact, such alliances are already in place. For instance, BMW, Daimler and Volkswagen are working with major German power suppliers such as Vattenfall, RWE, and Evonik. VW also recently began working with Toshiba on the development of battery technology. Powerful batteries are indeed the key to the entire vision, which is why their development has to be supported, said Thomas Rachel from the BMBF.
A total of €500 million could be spent on mobility research over the next three years within the framework of the German government's stimulus programs. Activities here could include the development of an appropriate infrastructure and all aspects of electric vehicle technology. Regardless of how the details turn out, conference participants emphasized that the overall goal is to make Germany the leading market for electric mobility.
Germany is already leading the way when it comes to electric mobility components for supplying energy or manufacturing electric automobiles. The country designs the most efficient power plants, whether conventional, wind powered, or solar-thermal—and has also developed systems for low-loss power transmission over great distances.
As far as automobiles are concerned, Germany remains a leader in electric motors and vehicle electronic systems. However, the situation is different with regard to battery technology. Here, most new developments are taking place in China and Korea; only around 1 % of all lithium-ion batteries are manufactured in Germany. Still, Germany has produced some new developments, as evidenced by the fact that a team of three scientists from Evonik's LiTec subsidiary was nominated for the German Future Prize two years ago. The team developed a separator for lithium-ion batteries that prevents short circuits, thereby making the high-performance units much more reliable. This is important because lithium-ion cells are regarded as being the only batteries capable of powering electric cars. Basically, they are the only batteries that can deliver the power density required for automotive transportation. The BMBF has thus established a "Lithium-ion Battery" alliance that will allow Germany to catch up in this field.
Tomorrow's Vehicle Alphabet
The term "electric mobility" is generally used to refer to personal transport in vehicles that are driven by an electric motor and/or are equipped with batteries that store a relevant amount of energy. These vehicles are classified as follows:
HEV = Hybrid Vehicle: Combination of an electric drive and a combustion engine
PHEV = Plug-In Hybrid Electric Vehicle: Hybrid vehicle with power-grid connectability
BEV = Battery-Electric Vehicle: Purely electric vehicle
FCV = Fuel Cell Vehicle: A vehicle that produces its own electricity through a chemical process
Many hybrid vehicles are already available on the market, and scaled-up production of all-electric vehicles will soon be launched.
At the same time, the BMWi has launched a "Mobility and Transport Technology" research program to develop state-of-the-art drive systems. Here, in addition to hybrids, the focus is on new power electronics systems for automobiles. A good electric vehicle requires a battery with an energy content of 42 kWh to achieve a range of around 300 km—in other words an energy consumption level of 15 kWh per 100 km. Assuming a normal voltage of 230 V and a current of 16 A, it would take around 12 hours to completely charge such a battery. "But at 400 V and 25 A, a driver could recharge in just two hours," says Professor Gernot Spiegelberg, who heads an electric mobility team at Siemens Corporate Technology. Every German household has 400-V potential because that's the voltage used by a normal three-phase current connection. "The only thing missing up until now has been a suitable interface between vehicles and the grid," he adds.
Spiegelberg's team, which works closely with Siemens' Energy and Industry Sectors, is the hub for the company's electric mobility research and development effort. The team's focus is on electric vehicle system requirements and the design of a mobility power grid infrastructure. Among other things, Siemens engineers are examining power generation and distribution options, transport and energy management systems, smart metering, power electronics, software, sensors and, of course, electric drives and the recovery and storage of energy. In addition to serving as energy storage units, electric drives could also become an important part of Siemens' Environmental Portfolio. That's because they utilize energy more efficiently than combustion engines.
"I believe that in Germany alone, there is potential for 4.5 million electric vehicles on the road by 2020," says Spiegelberg. "All of these vehicles could get their power from the existing grid. And that's just a conservative estimate, because these vehicles would only add up to about half of the second cars owned by families, most of which never travel over 70 km a day." As a consequence, one out of every ten vehicles in Germany would no longer use gasoline.
Germany is not the only country pursuing new electric mobility concepts; ideas are also being generated and implemented in the U.S., Australia, Israel, and Denmark, as well as in other nations. In California, a start-up called Better Place is addressing the entire value chain for a modern mobility system based on renewable energy sources. Launched two years ago, Better Place is working on the creation of a comprehensive infrastructure for the operation of electric vehicles. Following the concept used to attract mobile phone customers, Better Place plans to provide its customers with cars at discount prices—or even for free. Customers would then pay for the distances traveled, with their invoices based solely on the actual number of kilometers driven. Better Place believes it can provide customers with a better kilometer-based leasing deal for electric vehicles than can be obtained for a vehicle with a combustion engine. Here, battery stations designed like gas stations would enable batteries low on energy to be quickly exchanged for fully-charged ones.
Better Place has entered a partnership with Renault-Nissan and plans to work with local energy utilities to establish energy infrastructures in various countries. The first electric car-based systems are expected to be up and running by 2011.
German companies have also recognized the market potential offered by electric vehicles and are working hard to develop appropriate solutions. Daimler, for example, is looking to establish an alliance with energy provider RWE that would standardize battery charging stations. The fact that Abu Dhabi recently decided to become a major Daimler shareholder appears to confirm that the automaker is on the right track. Through Daimler, Abu Dhabi is banking on an accelerated transition from combustion engines to alternative drive systems, thus preparing itself for the "post-oil era." Similarly, BMW and Volkswagen are working with energy companies—among other things in order to determine which types of infrastructure are necessary for different mobility requirements. Their ultimate goal is to establish a foundation for the widespread introduction of electric vehicles.
The electric automobile revolution could end up taking place in Asia, however, as completely new players are now joining traditional automotive companies there. At the 2008 Geneva Motor Show, for example, a Chinese plug-in hybrid electric vehicle known as the "F3DM" was unveiled by a company called Build Your Dream (BYD). The car is equipped with a small-volume combustion engine (1.0 l displacement), a complete electric drive system, and a battery/storage unit that can be charged both internally via a generator and/or by exploiting braking energy recovery, or externally at a conventional 230-V outlet. The vehicle's range in the pure electric mode is 110 km, which is more than the average one-day requirement of most commuters.
On April 29, 1882, Werner Siemens drove the Elektromote—an electrically powered carriage—along a 540-m test track in Halensee near Berlin. Siemens' invention was not only the first electric vehicle, but also the world's first trolley bus. The Elektromote was followed in 1905 by the Electric Victoria, which rolled through Berlin as a taxi and delivery vehicle at a top speed of 24 km/h. Although these vehicles were well ahead of their time, their low battery capacities, speeds, and range couldn't compete with internal combustion engines. This state of affairs has lasted more than 100 years, and the rule of thumb even today remains that 1 l of gasoline equates to 9 kWh. A lithium-ion battery with that sort of content weighs around 100 kg. Still, an electric car can travel around 60 km on that energy, while a gasoline-powered vehicle will only manage 10 to 20 km. This range superiority is due to the fact that electric motors are roughly four times as efficient as combustion engines. Lithium-ion batteries are familiar as high-performance energy storage devices in cell phones, PDAs, and laptops. They can store two to three times as much energy as conventional nickel-cadmium batteries of the same weight. However, a €10,000 Li-ion battery would be required to power a passenger car that uses 15 kWh per 100 km. Mass production will thus be required to bring prices down to affordable levels.
In addition to energy storage technology, developers are also focusing on the drive train as a key electric mobility technology. In principle, drive trains for electric cars can be designed much more simply than is the case with gasoline or diesel engines because no transmission, differential, or drive shaft are required—a situation that is similar to that of 100 years ago when electric automobile pioneers built wheel hub motor vehicles. A wheel hub motor is a machine directly installed in the wheel, which means part of the motor turns with the wheel.
But unlike the mechanical systems of the past, the drive systems of the future will have brains. Intelligent electronic systems will manage components, charging and discharging procedures, as well as the brake energy recovery processes. And all of this will be designed to ensure that the energy efficiency, and thus the environmental soundness, of electric cars is much higher than the values achievable by combustion engines. The well-to-wheel efficiency (from energy source to operation) of a good electric vehicle today is over 70 % – based on renewable energy sources –, whereas the efficiency rating of most combustion engines is only around 20 %.
Even if the power for electric cars isn't generated from renewable sources such as wind and sun, the level of CO2 emissions from such vehicles is still much lower than that of any combustion engine. That's because power plants in the global electricity mix emit some 600 g of CO2 per kilowatt-hour, which corresponds to 90 g for every kilometer driven by an electric car. That's a lot less than the 120 to 160 g of CO2 emitted per kilometer by a typical mid-range automobile with a combustion engine.
Spiegelberg, who is a recognized expert in the field of electric drive systems, was instrumental in equipping two prototype vehicles with electric drive trains from Siemens. "At the Geneva Motor Show in March 2009, we presented our drive systems in the "iChange" concept car, which was built by Rinspeed, and in the eRuf Greenster, a vehicle produced by Alois Ruf," he says.
Rinspeed, a Swiss firm headed by visionary Frank Rinderknecht, is well-known for its forward-looking concept cars. Measuring around one meter in height and 4.28 meters in length, the "iChange" is equipped with a 150-kWh electric motor from Siemens Drive Technologies that allows it to accelerate from 0 to 100 km per hour in only 4.2 seconds.
The car's top speed is 220 km/h. However, when completely charged and operating at full output, the vehicle has a range of only 90 km. The car's lithium-ion batteries, which are produced by Gaia, a company located in Nordhausen, Germany, can be recharged in about three hours at a conventional electrical outlet.
In October 2008, Alois Ruf, a German company that specializes in modifying Porsches, presented an electric Porsche that it now plans to further develop with Spiegelberg. "For the prototype in Geneva, we used an integrated system consisting of a motor and generator, power electronics, and an interface with a battery connection," Spiegelberg explains.
The electric Porsche presented in Geneva by RUF Automobile GmbH contains a preliminary version of the innovative eDrive system from Siemens Corporate Technology. The prototype has a central motor with an output of 270 kWh and torque of 950 Nm. When driven in a moderate manner, it has a range of around 200 km. Ruf plans to manufacture a small lot of successor models that will employ a dual-motor concept. This so-called "eRuf" will be the first electric car in the world with a bidirectional power connection, which will allow it to be recharged within an hour at a 380-volt electrical outlet—without the extra electrical circuitry typically required for recharging. The bidirectional system will also permit it to feed energy back into the power grid via the same socket. A small group of the cars is expected to hit the road in 2010.
"As wonderful and powerful as these electric cars are, we mustn't forget that the vehicles themselves are just one link in an electric mobility chain," says Manfried Kruska, whose work in Siemens' Energy Sector focuses on electric mobility from an infrastructural perspective. Much still needs to be done here. For instance:
Siemens has years of experience and tremendous expertise in all aspects of the energy supply chain. The company is thus ideally suited to help design tomorrow's electric mobility system—from vehicle parts to power grid components.
With this in mind, when Tobias Wittmann from Siemens' Energy Sector attended the National Strategy Conference on Electric Mobility in Berlin in 2008, he presented a software program known as the "Vehicle-to-Grid Scenario." The software, which simulates the interaction between centralized and distributed energy systems, demonstrates the role electric cars will play as both energy consumers and energy sources. It illustrates how vehicles will be able to draw and store cheap electricity at night, and then sell the power back to the grid at a profit during the day.
Siemens' Energy Sector established a research alliance for such a system in February 2009, when it signed an agreement to join an international consortium in Denmark known as the EDISON project. EDISON stands for "Electric vehicles in a Distributed and Integrated market using Sustainable energy and Open Networks."
"The goal of the project is to standardize electrical energy-storage equipment and charging and discharging technologies for electric and plug-in electric hybrid vehicles," says Sven Holthusen, head of Siemens' activities in the consortium. "Our job is to study the potential for connecting electric vehicles to the public grid."
As a partner in the EDISON project, Siemens is responsible for coordinating and delivering key technologies, such as those needed for charging stations and associated control systems that ensure optimal utilization of battery capacities. At the heart of the overall setup are the power electronics and communication systems for managing battery charging and feed-in to the grid.
All of this plugs in smartly with Denmark's plans, which call for 50 % of its electricity to be generated by wind by 2020. As a result, the country sees the development of solutions for storing excess electricity as crucial. "If you don't utilize a storage option with wind, you need to install six times the normal output in order to ensure a sufficient and constant supply of power," explains Spiegelberg.
Klaudia Kunze
Connecting electric vehicles to the power grid poses a particular challenge, as large amounts of energy will need to flow quickly and in both directions if the electrical energy from batteries is to be used as so-called "regulating energy" during peak times. Regulating energy refers to the energy a power network operator must provide in order to offset frequency fluctuations in the network, which arise when more energy is being used than the base-load power plants are capable of supplying. Regulating energy then has to be supplied at short notice from natural gas plants, pumped storage hydropower stations, thermal plants, or energy storage units. "This is a challenge we are well equipped for," says Kruska. "We already have most of the components, systems, and solutions needed to establish an infrastructure to connect electric vehicles to the power grid. Our know-how covers switchgear, inverters, and control technology—but we also have network design expertise, SIPLINK for network coupling, and local grid transformers."
As new as some of this sounds, the associated Siemens innovations go back many years. In fact, the electric car is older than the combustion engine vehicle invented by Carl Benz in 1885/86. "The pioneering determination of our engineers to establish electric mobility has a tradition extending back more than 100 years," said Siemens CEO Peter Löscher at the company's Annual Meeting in January 2009. "After all, it was in 1882 that Werner Siemens presented the first electric vehicle, which he called the Elektromote. Today, electric vehicles have a much greater chance of becoming widespread than they did back then—at least in terms of urban transportation. What hasn't changed, however, is the pioneering spirit with which Siemens researchers and developers are working to achieve a major breakthrough for electric vehicles."
Klaudia Kunze
1 Energy suppliers integrate all forms of energy, from fossil to renewable, which is why intelligent power grids must be flexible and resilient.
2 An infrastructure consisting of charging stations and invoicing devices is established at public buildings and major parking lots.
3 Batteries in electric cars not only store electricity but return it to the grid if necessary. Internet-enabled cell phones are used to display all the key parameters regarding smart metering.
4 Electricity is traded like stocks, with each electric vehicle driver freely choosing to buy or sell, depending on the current price.
5 The electric car makes it possible to realize new vehicle concepts that include new electronic driver assistance systems that provide added comfort, entertainment, and safety. Service providers can utilize overarching standards to put together and market electric mobility packages. In such a setup, drivers don't purchase a car, but instead pay for the number of kilometers they travel.