Font Size


May 11; 2009 | In the future researchers at Forschungszentrum Juelich (Juelich Research Center) will be able to penetrate even deeper into the secrets of the brain — thanks to state-of-the-art imaging from Siemens. A large medical instrument that is unique worldwide was put into operation on April 29 at the research center. This new system allows detailed views of the interior of the human skull and can pinpoint the locations of pathological tissue and structural changes in the brain to within 100 micrometers. This is possible with a magnetic resonance tomograph (MRT) with a tremendous field strength of 9.4 tesla (almost 200,000 times stronger than the earth’s magnetic field) which will be combined later with a positron emission tomograph (PET).
The two constituent systems of this large-scale machine have different advantages. With the extremely strong magnetic field of the MRT scanner, the resolution of the images is substantially increased relative to a model with 1.5 tesla — the magnetic field strengths usually used in hospitals.
The PET scanner, on the other hand, can make brain activities and metabolic processes visible, which allows inferences to be made about tumor tissue. There are different kinds of PET examinations. Usually a patient gets injections of a very small dose of weakly radioactive liquid, which accumulates in cells with an elevated metabolic rate, for example. Positrons are released at these locations. Detectors record the radiation which results when positrons encounter electrons, making it possible to identify tumor cells on the basis of their metabolism. The Juelich researchers want to develop opportunities for diagnosis and therapy of brain diseases like Parkinson’s and Alzheimer’s, which up to now could not be treated or prevented. Foremost, they are researching the structure and the mechanisms of the brain in general. Siemens in turn hopes that this cooperation will make it possible to determine if there are new applications for MRT and for the combination of MRT and PET.
Reference Number: IN 2009.05.2e
Siemens Technology Press and
Innovation Communications
Mr. Dr. Norbert Aschenbrenner
Tel: +49 (89) 636-33438
Fax: +49 (89) 636-35292
norbert.aschenbrenner@siemens.com