Skip to Content

www.siemens.com
Siemens AG

Skip over Language Selection

Change language to

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Site Map & Contact

Site Map & Contact

Skip over Search

Intelligent Networking - Recipe for Success in the 21st Century

In an intelligent society, individuals communicate with each other, organize themselves and form networks. This paradigm is also utilized in modern technology and confers individual objects equipped with sensors, actuators and software a certain level of intelligence and identity. Through modern communications technology, single components are melded into an integrated network system. "Added value through intelligent networking" is one of the megatrends of our century and pervades all aspects of our lives. Networked technology improves the security of buildings and residences. It makes traffic flow more smoothly and increases the efficiency and flexibility of our health care system. There is almost no limit to technological progress: Microelectronics, wireless communications, sensor technology or new materials will be continuously improved. When these technologies converge, the result will be "smart objects" that are able to perceive their environment, process data and communicate with other objects.

 

Intelligent Networking: Forecasts

The "informatization" of the world is increasing rapidly. In the future, we can even anticipate an "internet of inanimate objects," predicted Prof. Friedmann Mattern of the Swiss Federal Institute of Technology (ETH) in Zurich. According to the German automobile club (ADAC), an automobile driver is caught in traffic jams an average of 65 hours per year. Especially in the traffic sector networked systems will play an important role in the coming years. The European market for telematic systems will expand correspondingly fast - a Frost & Sullivan study predicts growth from the present 3.7 billion euros to 5.8 billion euros by 2010. Today, already 1.1 million automobiles are equipped with integrated systems that combine infotainment features with parking assistance or emergency call systems. The analysts from Frost & Sullivan predict that by 2010 the number of these systems will increase to 6.6 million.

 
 

Intelligent Networking at Siemens

Very few other companies can match Siemens' exceptional know-how for the development of sensors, actuators, software or for information and communication technology. These technologies are the basis of intelligent networking and are already being applied worldwide - in self-organizing telephone networks and equally so in amusement parks or in industry. Intelligent networked video systems monitor the traffic and independently recognize fires in the Giswil Tunnel in Switzerland. In an emergency, the system triggers a chain reaction of alarm and safety measures and, through this, saves lives. In the Ruhr region, Europe's largest conurbation, Siemens technology enables collecting the information on the traffic density and the direction and speed of motor vehicles. From this data, a central computer determines the current traffic situation and transmits this information to motorists via radio, cell phone or internet. Networked systems from Siemens also ensure more safety and improved comfort in buildings. A good example is the T-Com House in Berlin. Here almost all electric equipment is interlinked with each other and can communicate with one another. All systems are centrally controlled via PDA - from the TV, lights and alarm system to the Venetian blinds, telephone and washing machine. In the tallest building in the world, the Taipei 101 tower in Taiwan, networked building automation systems from Siemens ensures the correct climate and security. These systems make the 500 meter tall skyscraper not only one of the world's safest buildings, but, in addition, reduce operating costs. The warehouses of large mail-order companies are networked with radio labels or RFID (Radio Frequency Identification) transponders from Siemens that make logistic processes more transparent and, hence, accelerate the flow of goods. At the moment, Siemens is the only company that offers RFID all-in-one systems.

 
 
 
 
 
 

Contact

Siemens Communica-tions for Technology and Innovations:

Dr. Ulrich Eberl (Mr.)
Wittelsbacherplatz 2
D-80333  Munich

Tel: +49 (89) 636-33246
Fax: +49 (89) 636-35292

ulrich.eberl@siemens.com