Skip to Content

www.siemens.com
Siemens AG

Skip over Language Selection

Change language to

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Site Map & Contact

Site Map & Contact

Skip over Search

New Light Sources

The development of new light sources literally makes a bright future possible. Today's lamps will become more efficient, smaller and, also, more environmentally friendly; for instance, mercury will be eliminated in high intensity discharge lamps. In adaptive lighting, different light sources, including daylight, will be combined and integrated into an intelligent network. Semi-conductor and organic light-emitting diodes are on the verge of a big breakthrough. Up until now the small dots of lights were mainly used as façade illumination and as display and indicator lights. In a few years they could replace conventional automobile headlights or contribute to the realization of flexible viewing screens.

 
 

New Light Sources: Forecasts

Even today, the range of applications for new light sources such as the high performance light-emitting diode is very wide and is continuing to grow. Likewise, the total global market for lighting is also increasing: the current market is worth 18.7 billion euro; by 2007, its worth will increase to 25.3 billion euro. In 2002 the world market for LED and LED modules alone came to 2.7 billion euro and was led by the two companies, Nichia and Osram, with 19 and 11 pro cent of the market share, respectively.

 

New Light Sources at Siemens

The Siemens subsidiary, Osram, is developing numerous innovative light sources for general and auto lighting. Light-emitting diodes (LEDs) are receiving special attention. The small dots of light produce electromagnetic radiation directly from the flow of electrons in semiconductors. With a light yield of up to 40 lumens per watt, LEDs are much more efficient than the common light bulb (6 to 12 lumens per watt) and are just under one square millimeter in size. The miniscule lights with the big effect are being used as automobile taillights and as flash units of mobile phone cameras. Future applications in high performance lighting functions such as automobile headlights or stadium floodlights are conceivable. Another type of LED possesses similar potential: OLEDs are composed of self-luminous, extremely flat, video-capable plastic and could, one day, revolutionize the market for displays. Also in development at Osram is a new lighting concept, which adjusts to the individual needs of a person. Depending on the time of day, the light from fluorescent lamps and LEDs are mixed to create an appropriate ambiance whereby the light spectrum is continuously modified. The goal is to increase the well-being and, thereby, boost the productivity of the consumer.

 
 
 
 
 

Contact

Siemens Communications for Technology and Innovations:

Dr. Ulrich Eberl (Mr.)
Wittelsbacherplatz 2
D 80333  Munich

Tel: +49 (89) 636-33246
Fax: +49 (89) 636-35292

ulrich.eberl@siemens.com