With the increasing complexity in technology, user friendliness for the consumer has become increasingly important. To address this point Siemens operates User Interface Design Centers in Munich, Princeton and Peking. At these centers, engineers, psychologists and designers study how products can be designed to best meet the requirements and wishes of the user. One result is the image processing software syngo from Siemens Medical Solutions. Forty-five Siemens medical technology systems, from x-ray apparatus to magnetic resonance imaging, have a standardized syngo user interface. The recurring design facilitates the application and use of the equipment.
The colored head-up-display developed by Siemens VDO Automotive should help the auto driver maintain a better overview of the traffic situation around him. This device is already being installed in the new BMW 5 series. The head-up-display projects relevant information such as vehicle velocity or navigation advice, with the help of several mirrors, onto the windshield. Thus, especially in difficult traffic situations, the driver does not have to regularly look down to the dashboard and can keep his attention focused on the road.