Siemens and the Feitoza foundation in Manaus, Brazil, are creating applications for cell phones that merge reality and the virtual world in real time.

Cuddly Combat is a new virtual reality game available on Siemens SX1 cell phones. It was created by developers in Munich in close cooperation with the Feitoza foundation—9,000 km away in Manaus, in the Brazilian rain forest


It may soon be the big hit among cell phone games: cartoon panda bears and similar creatures that crawl around in living rooms or on the street—but only virtually on a cell phone display. Dr. Alexandra Musto, head of a Multimedia Applications team at Siemens Com, describes the game which has initially been called "Cuddly Combat" as follows: "The 3D figures are set into the background in such a way that it appears as if they were walking around on the real table, for example. Players can zoom in on their mascots, turn them around and view them from above or below. The real backgrounds are recorded by the cell phone camera. Two players can play the game using a Bluetooth connection."
This combination of real and artificial worlds, which is known as augmented reality, is difficult to achieve even on a powerful PC. Implementing it in a cell phone, however, which has a relatively limited computing capacity by comparison, represented a major challenge. Nevertheless, the Feitoza foundation and Siemens managed to pull it off by working closely together. Specialists at Siemens designed the game’s concept and a catalog of image processing algorithms required for augmented reality applications. In order to merge the real world with artificial elements, the software has to learn to recognize the movements the telephone makes. The Multimedia Applications group has been working for years in this area. Among other things, it developed the algorithms for movement estimation that form the basis of the game known as "Mozzies" (mosquito hunt), which comes with the Siemens SX1 cell phone. This work also resulted in several important patents for such applications. The Feitoza foundation created and optimized procedures for compressing data as well as algorithms that ensure the game runs smoothly. The interesting aspect of this cooperative effort was that the Siemens experts did their work in Munich, while Feitoza made its contribution from Manaus, Brazil.
When asked why Siemens chose a company in Manaus as a partner, Bernhard Geisberger, director of PC Software at Siemens Com and head of R&D in Manaus, talks about the huge economic potential that exists in Latin American countries. "Only those who invest directly here can expect to participate in the region’s growth," he says. "All of this started with the establishment of a Global Support Center for the Java and Symbian community in 2002. Because that went so well, we decided to set up many other PC software partnerships, and then opened our R&D Center in Manaus in November 2003. We chose Manaus because there are a lot of highly motivated developers here and because the region offers financial benefits."
The designers of the new augmented reality game wanted it to be so real that players would not notice any difference between their real environment and its virtual supplement. To do this, the development teams had to combine methods from linear algebra, animation, rendering technologies and artificial intelligence and then depict them on the target platform—the Symbian operating system. Renato Lopez, director of Feitoza, says his organization not only had its team members take courses in fuzzy logic, neural networks and computer mathematics, but also had them conduct research into movement and collision detection and pattern recognition. All work has now been completed and the game is scheduled to become available soon in the SX1 cell phone and as a download version.
Some 160 of Feitoza's 200 employees work in R&D, most of them in projects involving Siemens. The foundation is a non-profit organization dedicated to promoting social development in the region through research projects. It supports 12 computer programming schools in the region and also develops devices for physically handicapped people. One of these devices is a special mouse. Here users control the cursor through eye movements and blink when they want to click on an object. The eye movements are detected by sensors attached to the user’s temples.
One aim of the cooperative activities between Siemens Com and Feitoza is to develop a globally valid platform for a cell phone manager. Such a system can synchronize contacts, e-mails, text messages and similar applications between a PC and a cell phone. The partners are also looking at software such as a processing program for images recorded with the cell phone camera.
The six-hour time difference between Germany and Brazil hasn’t been a problem; instead, it actually promotes efficiency. "It lengthens working hours," says Geisberger. While developing the software for the SX1 cell phone, the team in Munich sent its most recent version of the mobile phone manager to Feitoza in the evening. When the developers in Munich arrived at work the next morning the latest latest version from Manaus was already on their computers.


As developers in Munich are having lunch, their colleagues in Manaus are starting the day’s work. A few hours are available for joint conferences, then the Brazilians continue where Munich leaves off. The result: a workday with 16 productive hours
"Thanks to our partnership with Siemens, we have improved our knowledge in software development and also learned to work in global, multicultural teams," says Lopez. "Feitoza also gained experience and expertise in new areas of software development for the mobile communications sector and has become one of the leading software development companies in the rapidly changing cell phone market in Brazil."
According to Geisberger, development activities in Manaus focus on user interfaces for cell phones and PC software. Siemens has provided additional funding to further expand Java development activities in Manaus. It also searched for and found new partner companies, such as the Genius Institute, Fucapi and DBA. Genius, a non-profit research center in Manaus, specializes in voice recognition software and digital TV. Fucapi, which is also non-profit, analyzes hardware. DBA, a large, Rio de Janeiro-based software company, has some 1,500 employees and a branch office in Manaus. At the moment, innovative developments in the area of user interface design for next generation cell phones are being pursued in cooperation with a company called Quality. In addition, all partners are involved in setting up special education programs in cooperation with the University of Amazonas. It is thus clear that Manaus is gradually developing into a core location for research cooperation between Siemens and Brazilian institutions and companies.
Barbara Stumpp