Technology for the Environment
In Brief
▄ Several studies released in 2006 and 2007 confirmed that we face climate change brought about by greenhouse gases such as CO2, which are produced mainly through the combustion of fossil fuels. To ensure the effects remain manageable, the earth’s temperature must not rise by more than 2 °C. The global energy supply therefore has to be put on a new foundation that generates low amounts of carbon more at Trends, Facts and Forecasts and in the Interview with Prof. Schellnhuber
▄ All means have to be exploited to achieve this goal. Energy consumers will need not only more efficient solutions for heating systems, household appliances and lighting, but also energy-saving industrial motors and more fuel-efficient transportation. Energy producers, meanwhile, will have to focus on boosting the efficiency of their power plants and generating more energy from alternative sources such as water, wind, biomass, geothermal heat and waste. In each of these areas, Siemens has developed solutions that are already usable today more at Energy Efficiency, Building Systems, Energy from Waste, Energy for Tomorrow and Environmentally Friendly Transportation
▄ Siemens is also working on technologies for the future, such as fossil-fuel power plants that sequester CO2 and store it safely underground. Other developments include fuel-cell hybrid power plants that are designed to achieve an electrical efficiency rating of 70 %. This is 10 % more than the best combined cycle plant currently under construction. Siemens is also researching an extremely efficient automotive drive system in which the electric motors and brakes will be incorporated into the wheels
more at Power Generation, Fuel Cell Power Plants and Transportation
▄ Thanks to an in-house standard, Siemens systematically takes environmental factors such as energy efficiency and the prevention of harmful substances into account when planning new products more
▄ New solutions have also been developed for water purification. They range from sophisticated biological processes in which bacteria destroy the pollutants and chemicals are not required to plasma techniques which can eliminate substances that were previously non-biodegradable more
Business development & climate change
Dr. Georg Rosenbauer, PG
georg.rosenbauer@ siemens.com
Power plant technologies
Alfons Benzinger, PG
alfons.benzinger@siemens.com
Plasma treatment process
Dr. Werner Hartmann, CT PS
werner.hartmann@siemens.com
Dr. Thomas Hammer, CT PS
thomas.hammer@siemens.com
Berlin waste processing plant
Jürgen Knöfel, RD
juergen.knoefel@siemens.com
SIPAPER Reject Power
Dr. Hermann Schwarz, I&S
hermann.hs.schwarz @siemens.com
Fuel cells
Horst Greiner, CT PS
horst.greiner@siemens.com
Dr. Joachim Hoffmann, PG
hoffmannjoachim@siemens.com
Automotive technologies
Enno Pflug, SV
enno.pflug@siemens.com
Oslo subway
Walter Struckl, TS
walter.struckl@siemens.com
Low-emissions ships
Kay Tigges, I&S
kay.tigges@siemens.com
Product-related environmental protection
Dr. Ferdinand Quella, CT ES
ferdinand.quella@siemens.com
Sewage plants in Maryland
Susan McCorvey, I&S WT
susan.mccorvey@siemens.com
Osec-B-Pak
Alberto Garibi, I&S WT
alberto.garibi@siemens.com
Climate impact research pik@pik-potsdam.de
Sustainability at Siemens www.siemens.com/sustainability
Power Generation www.siemens.com/power
Institute for Climate Impact Research www.pik-potsdam.de