Mar 03, 2005
Siemens Medical Solutions introduces DynaCT for the first time in Europe at the ECR (European Congress of Radiology) March, 4th - 8th, 2005 in Vienna, Austria. This new application enables users of angiographic C-arm systems to create soft tissue images based on the principles of CT. These CT like images allow soft tissue differentiation that enables, for instance, detection of intracranial hemorrhages and visualization of the brain tissue. This in turn supports decision making during interventions. It is all made possible by modern flat detector (FD) technology from Siemens. The images on the picture are acquired with Siemens-system Axiom Artis dBA DynaCT without use of contrast medium.
Reference Number: MedAX200503008-04