Nov 17, 2005
Siemens’ CT Somatom Definition, is the first dual source CT worldwide with two x-ray tubes inside. It will provide clearer, more detailed images, lead to a wider ranger of clinical applications, and ultimately produce a higher quality of patient care.
The patient was admitted with atypical chest pain under exertion. A 6-second cardiac CT scan was performed to rule out coronary artery disease. The heart rate during the scan varied from 79 to 86 beats / minute.
Motion-free imaging of the left coronary and circumflex arteries. Even smallest side branches can be visualized.
Reference Number: MedCT200511019-04