Jun 14, 2006
Because the patient is suffering from chronic bronchitis and breathes in very short time periods the scan time had to be less than 10 seconds. The Somatom Definition with his two fast rotating detectors has a time resolution of 83 milliseconds. It took a pin sharp image despite the patients heart rate altered between 85 and 93 beats per minute during the scan.
Reference Number: MedCT200511019-05