Nov 17, 2005
Siemens’ CT Somatom Definition, is the first dual source CT worldwide with two x-ray tubes inside. It will provide clearer, more detailed images, lead to a wider ranger of clinical applications, and ultimately produce a higher quality of patient care.
Whole Body Run-off: The patient was scanned for suspicion of an aortic stenosis. In only 17s the scan range of 148cm was acquired and an aortic stenosis could be ruled out.
Reference Number: MedCT200511019-10