2007-Nov-14
At the Medica 39th World Forum for Medicine in Düsseldorf, Germany, Siemens Medical Solutions presents a new laptop-based ultrasound system, the Acuson P50, with integrated echocardiography software. The system is especially designed for mobile applications in cardiology as well as vascular applications and use in the operating room and anesthesiology departments. In addition to these functions, the P50 can be used as a standard Internet-enabled PC that also runs common office applications. With an array of transducers, the system lets physicians bring ultrasound anywhere it is needed.
Reference Number: Med US 200711.017-01