For the trade press
With its powerful 1.86 gigahertz Intel Mobile processor, the new Simatic Panel PC 577B from Siemens Automation and Drives (A&D) provides outstanding computing power for industrial applications. The panel, which is only 14 centimeters deep, has a main memory of 512 megabytes. This can be increased to up to four gigabytes. The diverse basic features of the Simatic Panel PC 577B include an 80-gigabyte hard disk, two Ethernet interfaces, a DVD burner, one USB interface on the front and four on the back, and two PCI extension slots. The touchscreen display is available in sizes 12, 15 and 19 inches. The panel PC has a high degree of protection of IP 65/NEMA4 on the front and is designed for temperatures up to 45 degrees Celsius. All versions of the PC 577B panel can be supplied ex warehouse.
Additional information is available on the Internet at: www.siemens.com/simatic-panel-pc
This press release is supplemented by a photo which you can view on the Internet at: www.siemens.com/ad-picture/1601
Gleiwitzerstraße 555
90475 Nürnberg
Tel: +49 911-895-7945
Fax: +49 911-895-7906
Reference Number: A&D AS 200710.1601e
Gleiwitzerstraße 555
90475 Nürnberg
Tel: +49 911-895-7945
Fax: +49 911-895-7906