2008-Dec-12
Siemens Healthcare redefined recently Magnetic Resonance (MR) in Oncology with Tim (Total imaging matrix) technology at the Scientific Assembly and Annual Meeting of the Radiological Society of North America (RSNA) in 2008. The company offers comprehensive and state-of-the art solutions for Oncology with MR. The software syngo Tissue 4D offers dynamic evaluation with quantification of tumor tissues in organs, such as the prostate and liver. Siemens introduced also new dedicated breast coils for 1.5- and 3-Tesla Tim systems. A second new breast coil for imaging and biopsy on 1.5 Tesla Tim systems is the Sentinelle Vanguard for Siemens. The next-generation breast MRI system Magnetom Espree – Pink was another highlight at the RSNA. The 1.5 Tesla system combines the 70cm Open-Bore design of the Magnetom Espree with the Sentinelle Vanguard solution. This breast coil offers exceptional breast imaging and biopsy access. The new system (picture) offers unmatched patient comfort, unique applications, and an innovative workflow pushing MRI Breast Care to the next level.
Reference Number: HIM200812014-01