2009-Mar-06
Siemens Healthcare exhibits its latest solutions in the field of Magnetic Resonance (MR) for Oncology at the European Radiology Congress ECR 2009 in Vienna. The syngo TimCT Oncology application enables not only comprehensive patient examinations within an extreme short examination time, it can also eliminate the need for multiple examinations with other modalities. The syngo Tissue 4D software supports tissue differentiation of prostate cancer (see picture). In addition, Siemens presents innovative technologies in the area of Women's Health: dedicated breast coils for 1.5 Tesla (T) and 3 Tesla systems as well as the new breast scanner Magnetom Espree - Pink. The 1.5T system combines a 70cm Open-Bore design with a dedicated breast care solution. Specifically designed for obese and claustrophobic patients, the large bore makes examinations more comfortable than with previous systems, or, in some cases, it makes them possible for the first time ever. Supplementary software packages such as syngo Grace allow for the biochemical detection of lesions that go beyond imaging.
Reference Number: HIM200903014-01