For the trade press
Nuremberg, 2008-Apr-08
Siemens Building Technologies (BT) is expanding its Gamma instabus range with the following three new devices for setting and controlling electrical installation systems: the Gamma N 305 scenic lighting/event module, the modular N 512/11 switch actuator and the N 151 IP viewer.
With the N 305 module, the user can recall up to eight different scenes or eight event programs such as "Presentation" or "Central off" that set the room or the building to a pre-defined state. This includes switching on and off, dimming of light sources, and heating control. Temperature sensors or any other sensors and events can trigger the relevant programs.
The N 512/11 switch actuator switches three outputs with 230 V AC and 16 A. The user can supplement the N 512/11 actuator with up to four expansion modules, and thus flexibly control 6, 9, 12 or 15 outputs. To replace at a later time, only the affected module needs to be changed. The switch actuator also has an integral scenic lighting control, status display, full local operation and load check.
With the Gamma N 151 IP viewer, the user's PC becomes the central switching and display element for KNX systems. The device functions as the interface between KNX signals and the LAN in the office environment. It can be used stand-alone as a operator panel and display unit. Any standard browser, whether on PC or PDA, can be used for display and operation. It is also possible to connect a centralized visualization system via the N 151 IP viewer.
A picture accompanies this press release. You can find this picture on the Internet at: http://www.siemens.com/ad-picture/1808
The Siemens Industry Sector (Erlangen, Germany) is the worldwide leading supplier of production, transportation and building technologies. With integrated hardware and software technologies as well as comprehensive Industry-specific solutions, Siemens increases the productivity and efficiency of its customers in the fields of industry and infrastructure. The Sector consists of six Divisions: Building Technologies, Industry Automation, Industry Solutions, Mobility, Drive Technologies and OSRAM. With around 209,000 employees worldwide Siemens Industry achieved in fiscal 2007 total sales of approximately EUR40 billion (pro forma, unconsolidated).
The Siemens Building Technologies (BT) Division, as a service provider and systems integrator and also as a manufacturer of the corresponding products, combines solutions and concepts for energy-efficient building automation, fire protection, electronic safety and electrical installation engineering. Due to this unique combination of activities, Building Technologies is a leading global player in the building automation market. The Division is an organizational unit of Siemens Schweiz AG (Zurich, Switzerland) and includes Building Technologies GmbH & Co. oHG (Erlangen, Germany), Building Technologies Inc. (Buffalo Grove, USA), their subsidiaries and holdings as well as all important Siemens activities in the field of building technologies.
Reference Number: I BT ET 200804.1808e
P.O. Box 4848
90327 Nuremberg
Germany
Tel: ++49 911 895-7950
Fax: ++49 911 895-7906