Industry Sector / Drive Technologies Division
Nuremberg, 2008-Aug-29
With the standardized and open interfaces of the Sinumerik 840D sl control, Siemens enables simple integration of robots into the shop floor area. Users of machine tools can use this to convert flexibly to automatic or series production in addition to standard tasks. Thanks to automated operation in loading machines with robots, for example, machine tools can also be used in non-working shifts, improving their utilization.
The economic necessity for higher machine utilization with simultaneous flexible change between customized production and automated series production are challenges faced by suppliers in the shop floor area. With the open interfaces of the Sinumerik 840D sl machine tool control, users can easily integrate auxiliary robots and can thus flexibly switch from operator-prompted production operation to automated series production during non-working shifts. The interface of the 840D sl is standardized, can be used immediately, and allows the connection of a host of industrial robots.
Industrial robots can be used for different additional tasks including loading operations, cutting, welding, or surface machining. By using robots for loading/unloading, machines can be better utilized and also operated during non-working shifts at night or at weekends. If the robot handles other additional tasks in machining, this reduces the overall cycle time and simultaneously increases production quality. The open interfaces of the Sinumerik 840D sl can be used to connect not only automatic lathes, milling machines and grinding machines to industrial robots, but also every other machine tool. One robot can also be used for several machines. This increases utilization, reduces the ROI of a machine, and secures the competitiveness above all of medium-sized production companies.
Operator-prompted production and automated series production are both based on the operating and programming tools ShopMill and ShopTurn. With these tools, machines can easily be configured, and the workpieces can be programmed via a graphical user interface. The changeover to automated series production is carried out in just a few steps. Siemens will present the integration of industrial robots in the area of shop floor production at the AMB exposition using the example of a Motoman robot.
You can find more information at www.siemens.de/sinumerik
A picture accompanies this press release. You can find this photo on the Internet at: www.siemens.com/ad-picture/1716
You can find the text on the Internet at: www.siemens.com/automation/presse
The Siemens Industry Sector (Erlangen, Germany) is the worldwide leading supplier of production, transportation and building technologies. With integrated hardware and software technologies as well as comprehensive industry-specific solutions, Siemens increases the productivity and efficiency of its customers in the fields of industry and infrastructure. The Sector consists of six divisions: Building Technologies, Industry Automation, Industry Solutions, Mobility, Drive Technologies and Osram. With around 209,000 employees worldwide Siemens Industry achieved in fiscal 2007 total sales of approximately EUR 40 billion (pro forma, unconsolidated). www.siemens.com/industry
Die Siemens Drive Technologies Division (Nuremberg, Germany) is the world's leading supplier of products and services for production machinery and machine tools. Drive Technologies offers integrated technologies that cover the entire drive train with electrical and mechanical components. This includes standard products but also encompasses industry-specific control and drive solutions for metal forming, printing and electronic manufacturing as well as solutions for glass, wood, plastic, ceramic, textile and packaging equipment and crane systems. The services provided by the Division include mechatronics support in addition to online services for web-based fault management and preventive maintenance.
Reference Number: IDT2008081716 en
Gleiwitzerstr. 555
90475 Nuremberg
Germany
Tel: +49 911 895-7946