For the trade press
Nuremberg, 2008-Dec-02
At this year's Euromold trade fair in Frankfurt/Main, Germany, the Drive Technologies Division of Siemens is exhibiting CNC solutions for all aspects of tool and mold making. The presentation focuses on the entire process chain of high-speed cutting and on solutions for the manufacture of medical implants and prostheses.
Meticulous machining and perfect surfaces are the primary prerequisites placed on the process chain involved in the machining of medical implants and prostheses. The extremely precise method of machining required here is based on an integrated, powerful CNC solution that encompasses CAD/CAM data generation, simple programming, setting-up at the CNC controller, matching probes, up to highly-accurate cutting with innovative tools. Siemens, together with its partner companies, DMG, Iscar and Renishaw, is showing solutions for high-speed cutting in medical engineering.
Meticulous machining and perfect surfaces are the primary prerequisites placed on the process chain involved in the machining of medical implants and prostheses. The extremely precise method of machining required here is based on an integrated, powerful CNC solution that encompasses CAD/CAM data generation, simple programming, setting-up at the CNC controller, matching probes, up to highly-accurate cutting with innovative tools. Siemens, together with its partner companies, DMG, Iscar and Renishaw, is showing solutions for high-speed cutting in medical engineering at Booth H36 in Hall 8.
High-speed cutting is a technically sophisticated cutting method. The CNC machines for such milling tasks feature high spindle speeds and much faster feed rates. These are the preconditions for the manufacture of high-quality medical products such as dental and bone implants, bone screws or hip prostheses. The Siemens Drive Technologies Division is demonstrating a variety of CNC solutions at Euromold, from CAD/CAM data generation with NX CAM to the system platform for high-speed cutting, the Sinumerik 840D sl controller with the Sinamics S120 drive system and powerful motors.
The Sinumerik 840D sl is the basis for complex milling tasks. The hardware and the software can be scaled separately from each other. With Sinumerik Safety Integrated, highly effective protection of both personnel and machinery can be implemented. The interplay of diverse functions enables the Sinumerik to flexibly adapt to changing requirements in CNC manufacturing. These functions include the simple measurement or calibration of multiple-axis kinematics as well as tool orientation. The jerk limitation and pre-control functions as well as the perfected look-ahead function support the operator in the set up and operation of machinery for tool and mold making.
The Euromold presence simultaneously marks the start of a roadshow of the Siemens Motion Control Systems and Siemens PLM Business Units together with the partner companies. DMG, Iscar and Renishaw will be giving live demonstrations illustrating innovative solutions for the manufacture of prostheses and implants with the help of HSC along the entire process chain.
You can find further information on the Internet at:
www.siemens.com/high-speed-cutting
A picture accompanies this press release. You can find this photo on the Internet at: www.siemens.com/ad-picture/1726
You can find the text on the Internet at: www.siemens.com/automation/presse
The Siemens Industry Sector (Erlangen, Germany) is the worldwide leading supplier of production, transportation and building technologies. With integrated hardware and software technologies as well as comprehensive industry-specific solutions, Siemens increases the productivity and efficiency of its customers in the fields of industry and infrastructure. The Sector consists of six divisions: Building Technologies, Industry Automation, Industry Solutions, Mobility, Drive Technologies and Osram. With around 209,000 employees worldwide Siemens Industry achieved in fiscal year 2008 total sales of approximately EUR38 billion (preliminary and unaudited). www.siemens.com/industry
The Siemens Drive Technologies Division (Nuremberg, Germany) is the world's leading supplier of products and services for production machinery and machine tools. Drive Technologies offers integrated technologies that cover the entire drive train with electrical and mechanical components. This includes standard products but also encompasses industry-specific control and drive solutions for metal forming, printing and electronic manufacturing as well as solutions for glass, wood, plastic, ceramic, textile and packaging equipment and crane systems. The services provided by the Division include mechatronics support in addition to online services for web-based fault management and preventive maintenance. With around 39,900 employees worldwide Siemens Drive Technologies achieved in fiscal year 2008 total sales of EUR8.9 billion (preliminary and unaudited).
Reference Number: IDT2008121726 en
Gleiwitzerstr. 555
90475 Nuremberg
Germany
Tel: +49 (911) 895-7946