Healthcare Sector / Imaging & IT Division
Hamburg, Germany, 2009-Sep-11
Adding a new premium ultrasound platform to its Women’s Imaging line of products, Siemens Healthcare introduces the Acuson S2000 ultrasound system – Women’s Imaging at the 19th World Congress of Ultrasound in Gynecology and Obstetrics (ISUOG) in Hamburg, Germany. At booth No. 201, the company demonstrates how innovative 3D/4D imaging solution and unique knowledge-based applications enhance the quality of care and speed up workflows in high-risk fetal imaging, obstetrics and gynecology as well as breast imaging.
The Acuson S2000 ultrasound system – Women’s Imaging represents the pinnacle of innovative technologies and workflow-enhancing clinical applications which dramatically improve the efficiency and quality of ultrasound exams. Latest acoustic technologies deliver a powerful system optimized for superb 2D, Doppler and 3D/4D imaging for the most demanding requirements in maternal-fetal medicine, OB/GYN and breast applications, including automated breast volume scanning. The system features unsurpassed image quality through 3D Dynamic TCE tissue contrast enhancement technology which sharpens borders and reduces speckle and noise in the entire volume – rather than in reconstructed “slices” only – to greatly improve subtle tissue differentiation for enhanced diagnostic confidence. Anatomic border definition and tissue contrast is additionally improved through Advanced SieClear spatial compounding and electronic beam steering which rapidly acquires overlapping images from different view angles.
Knowledge-based workflow applications
One of the highlights unique to the Acuson S2000 system –Women’s Imaging includes syngo Auto OB measurements, an advanced clinical tool that automates routine biometry measurements of the fetus. “Up until now, users needed to perform biometry measurements manually,” said Norbert Gaus, chief executive officer, Ultrasound, Siemens Healthcare. Syngo Auto OB measurements eliminate this time-consuming manual process saving up to 75 percent of the keystrokes in routine fetal measurements freeing users from repetitive tasks so they can focus on their patients.” The application also addresses the challenges related to user-dependence and variability, as well as consistency and reproducibility in fetal biometry. Measurements are automatically saved into the patient’s report and include the biparietal diameter (BPD), head circumference (HC), abdominal circumference (AC), femur length (FL), crown rump length (CRL) and the humerus length (HL).
Fetal Echocardiography
The Acuson S2000 system – Women’s Imaging also features advanced applications for fetal echocardiography. Syngo Vector Velocity Imaging (VVI) technology provides physicians with an advanced tool for the assessment of global and regional myocardial muscle and motion mechanics. Specially designed to analyze the delicate cardiac anatomy of the fetus, the application offers clinically valuable visual and quantitative data output including velocity, strain, strain rate, ejection fraction and volume. In addition, the new system features Fetal Heart STIC (Spatio-Temporal Image Correlation) imaging, which captures data over multiple heart cycles and creates a 3D fetal heart volume, allowing sonographers to view the fetal heart in multiple planes. “Obtaining a 3D volume of the fetal heart will allow easy interrogation of the anatomy and may help detect fetal cardiac anomalies more easily during routine obstetrical exams,” said Norbert Gaus, Chief Executive Officer of Ultrasound at Siemens Healthcare. “The earlier anomalies are detected and referred to a pediatric specialist, the better the clinical prognosis is for the postnatal infant.”
Advanced Volumetric Imaging
The Advanced fourSight technology package for the Acuson S2000 system – Women’s Imaging enhances diagnostic confidence by offering comprehensive 3D/4D data acquisition, data rendering and post processing including MultiSlice, Thick Slice imaging and inversion mode. 3-Scape real-time 3D imaging offers industry leading 3D/4D acquisition and multi-planar visualization. Real-time capture and display of grayscale and power Doppler volumes using both high resolution 2D and fourSight 4D transducer technology further enhance the solution. The system also includes industry-exclusive Amnioscopic Rendering, an advanced surface rendering tool which provides photo-realistic images of the fetus – a valuable tool to enhance maternal-fetal bonding.
Complete Breast Imaging Solution
The Acuson S2000 system – Women’s Imaging is open to integrate automated breast volume scanning (ABVS). This configuration features an innovative, mobile in-suite design combining the advanced Acuson S2000 system - Women’s Imaging with a transducer specifically designed for automated ultrasound breast volume imaging. Quickly acquiring full-field sonographic volumes for comprehensive review and diagnosis of the breast, it streamlines workflow and reduces operator dependence and variability. The advanced 3D technology enables the intuitive, anatomical coronal plane, not available using conventional ultrasound. This view provides a more understandable representation of the global anatomy and architecture of the breast. Semi-automated reporting and comprehensive BI-RADS reporting capabilities further enhance the clinical workflow. To further optimize high-volume patient breast care, the system also supports innovative breast imaging applications, such as fatty tissue and eSie Touch elasticity imaging.
Solutions for the Clinical Routine
The Siemens workflow solution for OB/GYN also encompasses the Acuson X300 ultrasound system, Premium Edition (PE) – Women’s Imaging. Compact, highly portable and easy to use, it offers sophisticated applications that were migrated from the high-end performance S Class into the X Class product series to support obstetrics, gynecological and breast imaging. Advanced fourSight volume imaging technology provides a complete 3D/4D solution in addition to delivering streamlined, intuitive workflow and advanced acquisition, data rendering and post-processing functionality for all examinations, including 2D and Doppler. The system also supports syngo Auto OB measurements addressing the workflow requirements of fetal biometry measurements. The Acuson X300 PE – Women’s Imaging accommodates the needs of any clinical environment – from private practices to busy hospital settings.
A press picture can be downloaded here:
http://www.siemens.com/med-pictures/AcusonS2000Women
The Siemens Healthcare Sector is one of the largest suppliers of healthcare technology worldwide. The company is a medical solution provider with core competences and innovative strengths in diagnostic and therapeutic technologies as well as knowledge processing, including information technology and system integration. With its acquisitions in laboratory diagnostics, Siemens Healthcare is the first integrated healthcare company that combines imaging and lab diagnostics, therapy solutions and medical information technology and also supplements these with consultation and services. Siemens Healthcare offers solutions for the entire supply chain under one roof - from prevention and early detection to diagnosis and to treatment and aftercare. In addition, Siemens Healthcare is the global brand leader for innovative hearing aids. Siemens Healthcare currently has around 49,000 employees worldwide and is represented in more than 130 countries. During fiscal 2008 (ending on September 30), Siemens Healthcare achieved a total sales volume of € 11.17 billion and incoming orders totaling € 11.78 billion. The Group earnings amounted to € 1.23 billion.
For more information, go to: http://www.siemens.com/healthcare
Reference Number: HIM200909.060 e TP
51 Valley Stream Parkway, H33
Malvern PA 19355
Tel: 1 610 448-1477