The highly modern production facility of OSRAM Opto Semiconductors in Regensburg, Bavaria, which began manufacturing optical semiconductor chips for light-emitting diodes (LEDs) in 2003, boasts an extremely efficient integral energy concept. Thanks to the combination of several totally different measures for optimizing energy utilization, the plant saves impressive amounts of energy with equivalent savings in CO2 emissions. This financially attractive concept is already being incorporated in the planning of the new chip production facility in Malaysia.
“Energy saving was already a high priority on the agenda before construction began in 2001 and was included in the overall plant concept from the very beginning,” explains Martin Stange, plant manager at the Regensburg facility, to visitors. At the moment he is showing a group of environmental protection officers from other OSRAM production operations around the plant, a brand new 56,000 square meter factory for semiconductor chips. He stops in front of a large green machine and explains: “That’s our absorption refrigerating machine. It converts hot 120-degree exhaust gases into cold air for air-conditioning.”
The Regensburg factory manufactures optical semiconductor chips, the core elements of LEDs. These tiny lights are one of the up-and-coming products of the future. They are small, rugged and light-intensive, and come in all colors. They are being increasingly used in the automotive industry, such as for dashboard lighting and for headlights, as well as in architectural lighting, street lights, cellphone illumination and wall displays. Since they convert electric power into light more efficiently than, say, conventional incandescent lamps, they play an important role in saving energy and reducing CO2 emissions. LEDs are manufactured from semiconductor materials in a highly complex process. The Regensburg cleanroom production site uses state-of-the-art chip and optical semiconductor production technologies, and the plant itself is a model operation when it comes to utilization of resources, transparency, operating reliability and minimizing environmentally relevant risks.
Small, robust and effective LEDs are now indispensable in many everyday lighting applications.
As Stange explains, the energy saving stipulated in the planning was systematically implemented. “Our approach was to group together different energy systems in the overall supply and disposal process at the location. For instance, we use waste heat from various manufacturing processes as well as the ambient cold air naturally present in the winter months. In the summer, excess process heat is additionally converted into cold air needed at this time of year for air conditioning,” he adds.
One solution is based on the principle of free cooling, which makes use of the latent energy in the outside air and is therefore used mainly in the winter or at night when temperatures are below 12° C. OSRAM uses the outside air to lower the temperature of the cooling water for the air-conditioning of the cleanrooms and the process cooling water. In the winter months, cold outside air is sufficient for cooling the entire facility.
In the winter months, hybrid coolers installed on the roof of the production hall use the surrounding air to cool the entire plant.
Since the free cooling process doesn’t provide sufficient cooling in the hot summer months, it is combined with a second process. This uses the cleaned 120-degree exhaust air. In the summer, this hot air is converted into cooling energy in an absorption refrigerating machine and is likewise used for cooling. In winter, the exhaust air is directly incorporated in the existing heating system via heat exchangers and used for preheating or postheating in the building’s air-conditioning systems.
Purified exhaust air is converted into cold air by an absorption refrigerator unit combined with an adiabatic cooling system.
Nevertheless, the two processes alone aren’t a comprehensive energy concept. That’s why the waste heat from nitrogen extraction is also used for the heating circuit in Regensburg. Nitrogen is needed for the production of semiconductors components, including LEDs, and was formerly delivered in liquid form by specialist companies. Now it is extracted directly from the ambient air at the production site. When operating, the extraction system compressors generate waste heat which can also be used for air conditioning. Another positive effect of producing nitrogen locally is that truck deliveries are unnecessary. For Regensburg plant, this has eliminated roughly 100,000 truck kilometers each year.
Nitrogen is obtained on the plant premises directly from the atmosphere. The compressor heat released in the process is taken up and used in the in-house heating circuit.
As Siegfried Schäffl, environmental officer and chief security engineer at the plant, explains, all these measures allow annual energy savings of about 13 million kilowatt hours (kWh) of gas and 4.5 million kWh of electricity. With the energy prices prevailing in mid-2009, this is equivalent to 858,000 euros, less the investment costs.
Siegfried Schäffl, the plant’s environmental officer and head safety engineer, can centrally monitor and control all the cooling systems and heating circuits in the entire plant.
“Our investment of about 1.7 million euros has consequently paid for itself within two years,” notes Schäffl, summing up as follows: “The legal requirements aside, we’ve designed and implemented a comprehensive energy concept at the Regensburg factory that considerably reduces energy consumption and thus the level of greenhouse gas emissions. This enables us to prevent the emission of about 5,200 metric tons of CO2 into the environment each year. It proves that our efforts have paid off – something we’re quite proud of.”