Climate protection must begin in the cities. The big cities consume 75 percent of the energy generated and emit 80 percent of the world’s greenhouse gases. They are thus the main culprit in terms of climate change, but they are also the place where climate protection measures will have most effect. The metropolises of the world can develop climate-friendly solutions which other regions can copy.
In the study commissioned by Siemens “Sustainable Urban Infrastructure: Munich – Paths toward a Carbon-Free Future” the Wuppertal Institute for Climate, Environment and Energy explored how the amount of CO2 emitted could be drastically reduced by 2058 – without impairing the quality of life for its residents. Using a specific model urban district, the analysis demonstrates how the transformation to a virtually carbon-free metropolis can be accomplished in terms of infrastructure and technology. Key levers for cutting CO2 emissions are high-efficiency energy applications, infrastructure modifications in the areas of heating, electricity and transportation and a transition to renewable and low-carbon energy sources wherever possible.
With the largest environmental portfolio in the world, which accounted for around €19 billion, or a quarter of total revenue in fiscal 2008, Siemens is ideally equipped to help achieve the necessary change.
The study is available as a download at
www.siemens.com/sustainablecities
and can also be ordered here.
The first part of the exhibition “Vision: A carbon-free Munich” shows the possible effects of climate change on world’s metropolises. The second part presents the findings of the study for the period from 2008 to 2058. According to the relatively optimistic Target Scenario, it will be possible to reduce emissions by around 90 percent to 750 kilograms per resident per year. According to the Bridge Scenario – based on more conservative assumptions about residents’ behavior – Munich will still be working towards becoming a largely carbon-free city. Nonetheless, CO2 emissions will have been reduced by 80 percent to 1.3 tons per person – and will thus still be much lower than the two-ton-per-person level advocated by the EU environmental ministers.
The third part of the exhibition shows on the basis of one model urban district how the levers that have been identified can help achieve this. It would theoretically be possible to reduce the CO2 emissions in an individual urban district to extremely low levels within a period of only 30 years. The study also shows that transforming a city into a virtually carbon-free urban environment can only be achieved if this aim is a top priority for all participants: decision-makers, bureaucracies, utilities, urban planners and, particularly, investors and residents. In the fourth part of the exhibition, various Siemens technologies are presented which help reduce CO2 emissions, ranging from power supply systems to electric cars and building management.